Hi all,
1) could someone let me know more details on the ADOVF / DAOVF flags in Register 1 (D7/D4)? The note on the "overflow flags" on page 24 doesn't really say why these bits are set - I assume it is because of exceeding input volatage? If not, then what does it mean when FIR/IIR "input range" is exceeded?
If they are not read, what happens to the data? Are they still valid? Is it just indicator or must me cleared? What happens if the user "dosn't care" about those bits?
2) Can this device work in programming mode only or it must switch to standard operation at some point of time?
best regards
OskarM.