I am considering an stereo 2-way active speaker project. Each speaker has three drivers: two woofers (4 Ohm) and one tweeter (4 Ohm). The electronic being considered is TAS5558 + TAS5176 x 2.
TAS5558 does EQ and crossover by its biquad filters at 192 kHz. Two TAS5176 are in BTL mode driving three drivers each. PWM1,2 of 5558 are connected one TAS5176. PWM7,8 of 5558 are connected to the other TAS5176. Two of the PWM inputs of 5176 are driven by the same PWM output of 5558 (for two woofers) as below. Is it a possible configuration?
5558 PWM1 -> 5176 PWM E/F (tweeter)
5558 PWM2 -> 5176 PWM C/D and PWM B/A (woofers)
5558 PWM7 -> 5176 PWM E/F (tweeter)
5558 PWM8 -> 5176 PWM C/D and PWM B/A (woofers)