This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

variable center frequency bandpass filter

Other Parts Discussed in Thread: LMF100

Hello, I need a bandpass filter design that has a voltage controlled variable center frequency from about 40Hz to about 10,000Hz with a high Q. Does such a filter exist? If it can't be voltage controlled then could it be controlled with just one pot?

I had thought to use the LMF100 switched capacitor filter but I need it with through hole pins and could only find it as a surface mount. 

I need 3 of these filters so I hope to find an IC or a simple circuit to use. 

Thanks!