Other Parts Discussed in Thread: PCM1792, DSD1792, PCM1792A, DSD1792A
HI , can anyone shed some light please:
Our customer developed a Portable audio player ,using PCM1792. and there are still some confusions.
[1] what's the difference between PCM1792 and DSD1792 ?
Dose PCM1792 support DSD64,DSD128,DSD256 ? if not ,which DAC product of TI can support ?
[2] When testing Idle Channel Noise , the results are quite different under test condition: ( 22Hz,22KHz,A-weighted ) and (22Hz,20KHz AES17).
And Under 22Hz,20KHz AES17 test condition, the Idle channel noise of TI's PCM1792 EVM is -111dB, while customer's device is only -108dB.
[3] When testing THD+N, only a few devices can reach 0.0004%, while most devices only 0.001%.
The testing signal is 1KHz , 24Bit , 0dBfs,44.1KHz sample rate Sine Wave.
FFT-LCH:
FFT-RCH:
signal:
THD+N:
Idle channel nosie under 22Hz-22KHz-A
Idle channel nosie under 22Hz-20KHz AES17