Hello,
I am new to the forums and was directed here by the TI Chat help. I'm designing a bluetooth speaker and need some help with amplifier board selection.
Here are my hard specifications:
1. 2.1 channel output with 5W left, 5W right, and 10W sub (all 4 ohms, although the 10W could be 8 ohm if necessary) (5W 4ohm speakers have already been sourced)
2. Can connect to Bluetooth (v4.0 or v4.1) chip (or preferably already had a Bluetooth chip integrated into it)
3. Accepts DC input, preferably 5.4V - 8.4V (I have already sourced a battery like this, but I source another if need be)
I am a biomedical engineer, but my background is in mechanics. I am just becoming familiar with electrical engineering through this project. I may need further clarification on technical details.
Sincerely,
David Eddy