Part Number: PCM5102A-Q1
Other Parts Discussed in Thread: PCM5102A, TS5A22364
Hello,
Unfortunately, I wasn't able to find this answer in the device datasheet. I'm adding an analog mute circuit to the PCM5102A because the XSMT functionality doesn't work like I need it to (I need L/R tied to AGND when the device is muted or otherwise not operational). I have decided to use the TI TS5A22364 SPDT analog switch which has negative voltage signaling ability for the task, but I'm not sure what the maximum voltage of the PCM5102A is (2.1v is what it's rated at, but what are the real world possibilities here). Additionally, I need to know what the voltage swing is.
I have also considered simply tying AGND to the normally connected pins of the TS5A22364 and leaving the normally closed pins N/C'd. That way, when music is not playing and the control pins on the switch are LOW, AGND will be tied to the L/R channels and I won't have to worry about passing audio through the TS5A22364.
Your input and information are greatly appreciated :).
-Ted