Other Parts Discussed in Thread: TLV320AIC3101
Hi,
I'm hoping to use the EVM GUI software on a Windows 10 system. Thus far I have:
- Downloaded the GUI software, slac249
- Installed using the "troubleshoot compatibility" workaround described in this TI forum post
- Downloaded drivers, slac521
- Installed both USB-MODEVM_WDM and USB-MODEVM_vista&7 drivers by disabling "driver signature verification", also detailed in the above forum post
- Plugged in the EVM, which articulates as an "unknown device"
- Manually updated the driver for the "unknown device"
- EVM now articulates in Device Manager
- NI-VISA USB Devices
- USB-MODEVM
I've made one change to the SW2, per section 2.2.1 of the User Guide (slau209a):
- Change SW-2.1 to ON
All other switches are in factory default position and match the recommendation of section 2.2.1.
Once I move SW-2.1 (A1) to ON, the LED at D2 illuminates.
I see the power LEDs in this state:
- D3: green
- D4: green
- D5: red
- D6: unlit
- D7: green
All other jumpers are in their factory default state. Specifically,
- JMP6 connecting pins 1-2 (USB)
- JMP10 connecting pins 3-5 (selecting I2C)
- JMP11 connecting pins 3-5 (selecting A0=0)
- JMP12 connecting pins 3-5 (selecting A1=0)
After launching the GUI software,
- Select AIC3106
- Select I2C
- Select A1=ON, A0=ON (for I2C address 0x36)
- Also tried A1=OFF, A0=OFF (for I2C address 0x30)
The software shows the dialog "Connect USB" - the GUI can't seem to find the USB device.
Do you have any suggestions on how to connect the device? I've tried several other switch positions but to no avail thus far.
Thanks!