This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3220EVM-MICRO: 3D Model and SCH/PCB design files

Part Number: TPA3220EVM-MICRO
Other Parts Discussed in Thread: TPA3220EVM

Hello!

I've got two requests, if possible:

1. I've got a TPA3220EVM-MICRO board that I'm evaluating and I'd like to build a 3D printed test enclosure for it. Is there a 3D model available that you could share with me? STL or STEP (STP) works great. It doesn't have to be extra detailed, the things that interest me the most are the connectors on the edge of the board (audio input jack, power supply and speaker out connectors) and as a nice to have, the two bulk caps for power supply bypass.

2. I already have a few ideas on how to modify the design to suit my intended application, and, if possible, I'd like to start by editing the EVM MICRO board schematic and layout, as most of the changes I have in mind are on the input side (well, at least for the beginning). So, can you please share the design files of the TPA3220EVM MICRO board (also, please indicate which tool can be used to view/edit the design files).

Best regards,

Andrei Carp