Hi team,
My customer has a question about TAS5825MEVM,Below is the question from the customer in verbatim:
"I have a question about TAS5825MEVM. I use an MCU to control TAS5825MEVM and start and initialize it according to the manual requirements, but the power amplifier has no output. I check the status register and find that the value of POWER_STATE register is 02H, which is the high resistance state. Please help to analyze, thank you very much! The values of other registers are as follows: CHAN_FAULT=00H, GLOBAL_FAULT1=04H, GLOBAL_FAULT2=00H, PVDD_ADC=7.12V, DEVICE_CTRL2=03H, FS_mon = 0BH, BCK_mon =40H, CLKDET_STATUS=08H"
Thank you very much.