I'm looking for an example of the profile configuration for the TAS5722L.
in the datasheet, it has the detail and register map but I can not find the example for the configuration
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
We typically do not provide such examples if it is not in datasheet. Let us check if there is examples available.
BR
Hello Saran,
The register map is very simple for this device and the default register values are loaded during the power-up sequence or any time the DVDD voltage falls below the power-on-reset (POR) threshold and then returns to valid operation, so we don't provide an example config.
Please refer to the register map in the datasheet if you want to make additional changes to the configurations.
Best regards,
Luis