This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TI Cable Equalizer - DS30EA101

Intellectual 430 points

Replies: 1

Views: 312

Hello,

In regards to LVDS buffer/equalizers, P/N: DS30EA101 and DS30BA101, the input spec for the ‘EA101 says 720mVp-p min at 0m cable length.  What is minimum with say 5m cable or 10m cable?  I’m wondering if they need to set their voltage drive level a little higher.  The data sheets show an example which they used.

Thanks,

Mehrdad.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.