Q1:
LMX2492 Data Sheet p28, the EVM is designed with PLL parameters (Kvco=200MHz/V, BW=380KHz, R=1, N=96, Kcp=??, Fin=100MHz, VccCP=5V) resulting in loop filter R's and C's listed in the table.
Entered the PLL parameters into Clock Design Tool I don't get the EVM Loop filter Cap and Resistors values listed. What is the reason?
Q2:
Also I would like to transition to an active filter(LM6211) to accommodate a wide band VCO with low Kvco=50MHz/V and a wider tuning range 0 to 15 Volts. How is an Active filter design entered into Clock Design Tool? How will it cover the tuning range since VccCP=5Vmax? What Kvco value do I enter (50MHz/V or 3*50MHz/V) into the VCO section of the Design Tool?
Thanks.