I want to use cdclvd1212 to transfer one signal with 2 second period .
But I find that the output signal of cdclvd1212. So, is the frequency too low to transfer?
intput: LVDS
output: LVDS
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to use cdclvd1212 to transfer one signal with 2 second period .
But I find that the output signal of cdclvd1212. So, is the frequency too low to transfer?
intput: LVDS
output: LVDS
I don't see an issue using the CDCLVD1212 in this use case. However I would recommend that you use only DC coupling.
wangzhi said:But I find that the output signal of cdclvd1212. So, is the frequency too low to transfer?
73,
Timothy