Other Parts Discussed in Thread: LMK00308,
Hi,
- A 100MHz LVDS (4-mA HSDS or 6-mA HSDS) clock is generated from LMK04610 and is fed as input to the LMK00308. The differential output voltage swing is much higher than the normal LVDS specification so what on board termination have to set at the LMK00308 input? Does a single 100E resistor with AC coupling termination is sufficient?
- If 8-mA HSDS or 16-mA HSCL output configuration is selected accidently, then will it damage the CLKIN pins of LMK00308?
Thanks in advance
DEEPAK V