This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2581: LMK00308 DRIVING LMX2581

Part Number: LMX2581
Other Parts Discussed in Thread: LMK00308

Hi,

I would like to drive lmx2581 using lmk00308. Is it good to add clock buffer to convert differential to single ended or using reference design from EVM ?

If second option is preferred, lmk00308 differential output is converted to single ended using the reference circuit given snau136c.

But for lvds outputs of lmk00308 VOD = 400mv & vos=1.25V , will this be sufficient to drive OSCIn of lmx2581 which requires an AC coupled input of min : 0.4vpp to max :1.7vpp after i convert differential output to single ended as suggested in EVM instructions

snau136c.pdf