Greetings,
I have some questions I hope someone could answer.
these are as follows:
* does the part support spread spectrum?
* I am using both banks but I will not be using all outputs.
what is the best way to terminate LVDS unused outputs?
* I have two signal inputs coming in, one is a LVDS signal from an oscillator EG-2102CA and the other is HCLS.
Since the LMK00306 doesn't have any internal termination resistors, then that means I don't need the SC coupling capacitors for the LVDS input signal correct?
also would I need the 50 ohm resistors that tie to ground for the HCSL signals?
thank you in advance