In addition to syncing parts, I would like to send some configuration information on a SYSREF clock by controlling it with the SYNC/SYSREF_REQ pin using an FPGA GPIO pin (see "9.3.2.2.3 SYSREF Request" in the datasheet). I plan to set SYSREF_PULSE_CNT to zero, so that it will generate just one pulse per SYNC/SYSREF_REQ event. I plan to set SYNC_1SHOT_EN to make it level sensitive. I need to know setup and hold time requirements for the SYNC/SYSREF_REQ pin to make this strategy work, but that information does not appear to be in the datasheet. Is it possible to do what I want to do here? What additional information do I need to make it work?