This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2592EVM: USB2ANY Firmware Update

Part Number: LMX2592EVM
Other Parts Discussed in Thread: USB2ANY

When I plug in the brand new USB2ANY I received with the board, it asks for the firmware update

 - Unplug USB2ANY

 - push BSL button and plug back in

 - Firmware update button appears

 - Always fails with "Memory Verification Error"

At least 5 attempts.  Windows 10.

  • James,

    There are 3 things I could see:
    1. Issues with Windows 10. '
    In our lab and here we use windows 7, so I can't verify your issue with USB2ANY.
    Is there any way to try this on Windows 7? This is very stable on windows 7.

    2. Damaged USB2ANY
    There are some ways you can mess up the USB2ANY, and I have done it. For instance, if you hold down the BSL button and don't let go of it and do the software update, then it can mess up the USB2ANY.

    3. Improper technique
    When you do the update, unplug the USB cable, push the BSL button, then plug in the USB cable. Then after it recognizes this, let go of the BSL button (I don't think it always says to do this) and then do the update.


    Regards,
    Dean