Other Parts Discussed in Thread: LMK00301
Hello team,
My customer would like to know if below connections work correctly.
OSCin: Pin. 12 > 51ohm > 0.1uF > GND
OSCout: Pin. 13 > Non connected.
REFout: Pin. 33 > Non connected.
Q1. Any problem for these connections?
In addition, there is the sentence in the datasheet below.
"When REFout is disabled, the use of a resistive loading can be used to set the output to a predetermined level.
For example, if REFout is configured with a 1 kΩ load to ground, then the output will be pulled to low when
disabled."
Q2. What does "the output" refer to, REFOUT or CLKOUTA/B?
Q3. Initially REFout: connected to GND via 1Kohm, but if it affects the output drop of REFout, please let me know the right way when unused.
Q4. What is "DC" for MIN of fCLKin in the datasheet P8?
Thank you for in advance for your cooperation.
Regards,
Kurita