Team,
Thanks for usual prompt support.
Please support below two inquiries from our customer,
1, Is there a problem with the following pin?
OSCin: Pin → 51ohm → 0.1u → connected to GND.
OSCout: Floating(free pin)
REFOUT: Floating(free pin)
2, Datasheet on page21, What is the output of the following sentence that is described below? Do you mean REFOUT? Or is it CLKOUTA / B?
"When REFout is disabled, the use of a resistive loading can be used to set the output to a predetermined level.
For example, if REFout is configured with a 1 kΩ load to ground, then the output will be pulled to low when
disabled. "
Initially, the customer was designing a circuit with 1 kohm → GND connection to REFOUT,
If the output level of CLKOUTA / B goes down, it is not the expected behavior,
Please let me know the correct unused process.
Thanks
Best regards,
Shidara