Other Parts Discussed in Thread: LMK00304,
Hi All,
I am sending this email to ask some questions on input bias voltage and termination resistor of LMK00304/08.
My customer has applied LMK00304 and LMK00308 to new system and they are used for LVDS interface.
Customer said that the datasheet recommends to place the termination resistor before the AC coupling cap.
However, they found that the input bias voltage on both inputs is different when they measured the waveforms of LMK00308 input. After changing the placement of termination resistor to behind AC coupling cap, the bias voltage became same on both inputs. Please find the attached to see the scope captures.
Regarding the placement of termination resistor, they have some questions.
Please refer to below comments, would you answer those questions?
- Why do both inputs have the different bias voltage when the termination resistor is placed before AC coupling? Could the output pins supply the normal waveform even if there is the difference on bias voltage?
- Looking at the attached file, both inputs could have same bias voltage after changing the placement of termination resistor behind AC coupling cap. Could the termination resistor be placed following AC coupling as customer modified? Please let me know if you have any concern on this placement.
- The datasheet states that the CLKin input has an internal bias voltage of about 1.4 V but you can see the bias voltage is 1.2V from the scope capture when placing the termination resistor behind AC coupling cap. Could you let me know why input bias is fixed as 1.2V not 1.4V?
LMK00304 terminated resistor_040319.pptx
Thanks in advance.
Best regards,
Sammy