Hi,
The datasheet Abs Max states VOSCin can handle up to 1Vpp with Vcc = 0V. Is this the case for each pin 8 and pin 9, separately (S/E) or together (differential)? For example, if VOSCin is driven S/E, does this mean that OSCinP (pin 8) can handle up to 1Vpp (4 dBm)?
In case the 1Vpp limit is for the case in which VOSCin is driven differentially, what is the Abs Max for the S/E case?
Thanks,
Marjorie