This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00334: Questions

Part Number: LMK00334
Other Parts Discussed in Thread: CDCM9102, CDCI6214

Dear *,

we need to provide clk for PCIe gen2 or gen3.

We would like to use the LMK00334 with differential 100MHz oscillator, and have some questions.

1) is there a difference if terms of signal integrity and quality or any other difference  if we use LMK00334 + LVDS 100MHz differential oscillator to [ CDCM9102 + 25Mhz oscillator or CDCI6214 + 25MHz oscillator]?

2) what is the proper connection [ termination] if we provide LVDS clk to LMK00334 input, or LVPECL clk to LMK00334?

3) what kind of HCSL driver is the output driver of the LMK00334 ?

a) standard HCSL current drive

b) LP-HCSL push-pull 

4) What is the output impedance of the HCSL driver?

5) if the HCSL is push-pull does it also include internal series termination?

6) When do we need the Rs series termination  and Rt termination and when not? Because on the EVM the Rs is set to 0R and Rt is set to DNI ?

7) if the LMK00334 transmitter provides clk to pcie device [ eg intel i210] can the clk bi direct connected without terminations if the i210 has HCSL receiver?

8) what is the preferred differential impedance for PCIe clk gen2 and gen3? we know that the PCIe data RX/TX should be routed at 85Ohm.

Best Regards,

David.

  • A1. I do not anticipate a major difference in performance.

    A2. DC-couple the LVDS or LVPECL input to the device. For LVDS, use a 100-ohm external load at the LMK0334 input. For LVPECL, 

    A3. The LMK00334 HCSL output buffer is a current drive output.

    A4. Due to the current drive nature of the output, it is effectively Hi-Z.

    A6. Rs typically ranges up to 33-ohms. Rs can be placed to dampen reflections. HCSL requires a 50-ohm termination to GND (Rt).

    A7. Your understanding is correct, if the receiver has the termination integrated, you would not need to place external terminations.

    A8. Our clock devices are designed for 50-ohm single-ended traces, or 100-ohm differential.

    Kind regards,
    Lane