I'm working with the ZCU111 Board to generate a 125Mhz clock. The board came with a VCXO of 122.88Mhz and a 12.8Mhz reference. ZCU111 was modified to use 125Mhz (50 ppm) as VCXO and was provided a 10Mhz reference (100 ppb) at CLKin0. The LMK04208 is used as a jitter cleaner with the 10Mhz reference and the VCXO for jitter cleaning. The register configurations were generated using the TICS Pro tool v1.6.10.0. I have pasted the values below. The tool showed 125Mhz.
However, with a frequency counter, clock output measured at CLKout2 is 125MHz, with a +30 PPM. Is there any guidance you can provide on programming the LMK04208 to get the actual 125MHz without so much drift?
R0 (INIT) 0x00160040
R0 0x00143200
R1 0x00143201
R2 0x00140302
R3 0x40140023
R4 0x40140024
R5 0x80141E05
R6 0x01100006
R7 0x01100007
R8 0x06010008
R9 0x55555549
R10 0x9102410A
R11 0x0401100B
R12 0x1B0C006C
R13 0x2302806D
R14 0x0200000E
R15 0x8000800F
R16 0xC1550410
R24 0x00000058
R25 0x02C9C419
R26 0xAFA8001A
R27 0x1000179B
R28 0x004125DC
R29 0x0100031D
R30 0x0200031E
R31 0x003F001F