This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CDCLVD1204: To confirm the recommended power supply decoupling method in the datasheet

Prodigy 10 points

Replies: 1

Views: 94

Part Number: CDCLVD1204

Hi colleagues,

According to the datasheet, the recommended power supply decoupling method is to use a 1uF capacitor on the board supply side and 10uF + 0.1uF capacitors on the chip supply side. It is not a typo, right?

I have checked the design of the EVM of CDCLVD1204. 4.7uF is used on the board supply side and 4.7uF + 0.1uF are used on the chip supply side. 

A similar strategy is deployed on the EVM of other ICs in the same family, like 10uF on the board supply side and 10uF + 0.1uF on the chip supply side.

It would be grateful that you can confirm the recommended power supply decoupling method for CDCLV1204 here. Many thanks in advance!

Best Regards,

Qipeng

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.