Other Parts Discussed in Thread: LMK00105
Hi,
I have a question regarding LMK00105 EVB that I've received recently.
I've noticed that on the board (see scan attached) at the Clkin and Clkin* lines there are:
- 0 OHM resistors at C9, C11 locations , while according to the schematic there should be 0.1uF capacitors.
- Capacitors at R6, R10 locations, instead of 0 OHM resistors
It seems that the components were swapped during the manufacturing (manufacuring error) .
I just need a confirmation for that.
Best regards,
Vitaly