Hello TI Experts
I'm struggling with the LMX2594 which at some frequencies sometimes randomly outputs a spur.I have two LMX2594 as LO's in a double superhet receiver. First I thought this was leakage and cross products. However, the problem appears also if I only run the LMX2594 alone (no other components running apart from external refclock).
The following examplifies the issue: I have the LMX2594 set to 7.097GHz with a reference clock of 143.36MHz. The registers I use for programming are attached.
I dump the registers to the device and sometimes the result is with spur at 400kHz offset:
Then after re-programming with the same registerfile the result is without spurs:
Attached also phase noise measurement results: phasenoise_lmx2594_nok.pdfphasenoise_lmx2594_ok.pdf
In both cases the device reports a "Locked" state.
Any help with this issue is very much appreciated!
Registerfile: (decimal)
LO1 Registers LMX2594 ======================= 7340032 7274496 7208960 7143424 7077888 7012352 6946823 6881280 6815744 6750208 6684672 6619136 6553600 6488064 6422528 6359040 6291456 6225920 6160384 6094848 6029312 5963776 5898240 5832704 5767168 5701632 5636096 5570560 5505024 5439488 5373952 5308416 5242880 5177344 5112075 5046272 4980748 4917248 4849664 4784191 4718596 4653185 4637520 4521984 4457448 4390912 4325876 4259840 4199304 4128768 4064034 3997864 3933160 3866625 3833857 3735584 3670016 3604480 3538944 3473408 3409952 3342464 3276800 3228032 3146496 3080960 3016700 2998514 2896419 2818205 2752512 2686976 2621440 2556416 2490368 2425860 2359365 2301473 2228224 2170401 2098067 2032620 1978764 1913228 1836168 1769474 1707440 1639972 1574682 1507452 1441793 1377281 1357896 1255351 1179748 1114414 1048704 984655 925296 868352 806919 720920 660184 595460 532480 458930 444418 327880 264771 198210 132352 67592 9628