This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Weidong,
The LMK01801 has two inputs, so I see no issue with cascading these. I think that because it is derived from the same clock, crosstalk between banks should not be an issue. I think that it is best this way as you have it to drive CLKin0 from CLKout12, because the smaller divider likely has better noise floor and will help divide down the noise of the bigger divider.
You should also be able to put a mux before CLKin1.
The only thing to be careful with all these dividers is that if the frequency gets too low, make sure that you don't violate any specs. Also, if you have an AC coupling capacitor, make sure it is of sufficient size.
Regards,
Dean