Other Parts Discussed in Thread: LMK04208
Hello,
I am quite beginner with PLL's neither have strong theory background. So i would like to know some basic stuff. We have the ZCU111 evaluation board with LMK04208 and three LMX2594. As i can understand the LMK04208 feeds the with 122.88MHz (in the current setup) LMX2594 PLL's to produce the RFdac-adc required frequencies. I have downloaded the TICS Pro tool (which is a very helpful tool ) to produce and export the required registers for the LMX2594.
So , in case i want i.e 250MHz instead of 245.76MHz (the second is an easy frequency to produce because it needs integer PLL , please correct me if i am wrong) should i make the PLL fractional or should i programm the LMK04208 to the appropriate frequency to have again integer PLL in LMX2594? Are there any disadvantages using fractional PLL? Which is the best of the two ways to achieve the desired PLL frequency?
Thanks in advance,
Your sincerely,
Theo Kontogiorgis