This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPL5111: TPL5111

Part Number: TPL5111
Other Parts Discussed in Thread: TPL5110

I am using TPL5111 in my project (was considering TPL5110 originally)..

What i experience testing this is somehow odd...

I set TPL5111 in ONE SHOT mode and have a 20K resistor installed to set time to aprox 50sec. It seems to work fine and on time. I press the button to trigger the timer DELAY/M_DRV pin and it turns on for 50sec give or take.. if a DONE signal comes in sooner, it turns off and stays off until another manual activation which is i suppose how its supposed to work.

the problem is when setting the chip to work in TIMER mode.

what i get is, it will turn on after powering up and will stay on until it receives a DONE signal. Then it activates again but the time before it does is not the same every time and it varies from 40-47sec

Is this normal to get such variation?