Hello,
Could you kindly help on the questions below, thanks?
1. Use REF1 for 25MHz reference, but it is 24.9999MHz, do you think this will cause the output frequency is a bit lower than set?
2. How many methods to fine-tune these output frequency? Could change the fraction-divider works? any other method?
3. If I change the fraciton-divider register while the PLL working, will the setting active immediately? or I need power on reset?
Thanks.