Hi,
I'm trying to configure LMK05028 to generate a 10MHz output from a 1PPS reference signal coming from a GPS receiver. The configuratio is the following:
XO: 48MHz
TCXO: 10MHz
IN0: 1PPS
OUT0: 10MHz from DPLL2
DPLL2 Mode: 3-loop
I attached the .tcs file in order to let you have a deeper look to my configuration.
On OUT0, I get 10,000,003MHz rather than 10,000,000MHz; after some tests, it seems that the component do not correctly locks to the 1PPS input: infact, the 10,000,003MHz output is present even if the GPS receiver is not connected.
What would you suggest to solve the problem?
Best Regards,
Michele