I have begun to have a look at LMK05318 I2C communication. The goal is to store in a memory 8 sets of registers. Then, based, on a input given by the end-user, these values will be written into LMK05318 registers through I2C using a microcontroller. For now, however, I am using LMK05318EVM in order to power and to program the registers.
The first doubt is about LMK05318 address. According to "LMK05318EVM User's Guide" (page 16) when S6[1:3] = 001, the address should be 0x64 . However, when I issue the command "Scan I2C bus" with TiCS-Pro, the following output is given " Device found at 0x78. Address will be updated" I have only this EVM connected to the USB and there are no communication issues between TICs Pro and the EVM
Moreover, I have put a logic analyzer in order to observe I2C communication when TICS Pro commands are sent to the EVM. For example I issue the command "write single register" with TicsPro in order to write the register R319 with the value 0x03. The values returned by the logic analyzer are 0xF0 0x01 0x3F 0x03. Therefore, considering the first byte 0xF0 and the shifting, I guess that LMK05318 7 bit address is 0x78 because after the shifting into 8 bit address this value becomes 0xF0.
What I am missing? Thanks in advance