Can the STAT1 and STAT0 outputs be programmed to be 3.3-V LVCMOS when selected to report Loss of Lock and/or Loss of Signal? If so, how is this selected/ set in the registers?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can the STAT1 and STAT0 outputs be programmed to be 3.3-V LVCMOS when selected to report Loss of Lock and/or Loss of Signal? If so, how is this selected/ set in the registers?
The STAT0 and STAT1 outputs are controlled by several registers (R13-17, R19, R27, R28, R45, R56). Use the TICS Pro GUI to easily configure the register settings for LMK03318. The GUI also works with LMK03318EVM if you plan to test on the evaluation module.
Kind regards,
Lane