Hi team,
1080i, 59.94 Hz horizontal synchronization created from a fixed oscillator (27 MHz) is input to HIN after power up.
The register settings are the device default settings.
When the HIN is input, the NO_LOCK pin is supposed to be L . But in some boards, NO_LOCK does not go to L.
Since NO_LOCK is monitoring the status of PLL 1 through 4, I read the status register.
PLL 2, 3, and 4 were locked but PLL1 was not locking.
Is it correct that only the HIN input is needed for PLL1?
There was no change when I put VIN for testing.
I checked the external 27M-VCXO is working.
Best Regards,
Itoh