Hi Team
My customer is using PLLatinum Sim Tool for LMX2594 simulation.
He has two questions when using it.
1. About Phase Margin
[Simulation condition]
Select device: LMX2594
Filter designer: Auto
Fpd: 200MHz
Fvco: 15000MHz
The customer said, the calculation result (Actual) is displayed as 70deg,
But from the bode plot between open loop gain and phase margin, the phase margin didn't seem like 70 deg.
When only look at peak value of phase margin, it looks close to 70 deg. So is that a bug that horizontal axis shifted?
Or "Actual" value of phase margin means just the peak value?
2. About LoopFilter Components C3
[Simulation condition]
Select davice: LMX2594
Filter designer: Fixed to LMX2594EVM constant value(forced component)
Fpd: 200MHz
Fvco: 15000MHz
There is an alert about loop filter component C3(the background becomes yellow).
After confirming the alert statement, it says "The capacitor closest to the VCO is less than 3.3nF, which could result in some degradation in VCO phase noise performance, and this is not modeled by the simulator".
Since the customer set the filter designer to "Fixed to LMX2594EVM constant value",
so the customer is wondering why the EVM would use a constant value like this even though it shows alert.
I am sorry but I am not familiar with PLLatinum Sim Tool, I tried to explain the question understandable.
If you need any other further information to solve the question, please just tell me. Thanks.