This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPL5110: DRV out to be maintained active

Expert 3795 points
Part Number: TPL5110

Dear e2e support,

If my understanding of our TPL5110 is correct, the DRV output remains active during a maximum of "Tip-50ms".

Is there a solution to maintain this output always active?

My need is to add a delay between an external event and a relay we have to drive:

external event --> delay set between 0 and 2s --> drive a relay until we decide de reset the function.

Do you see any trick to do this with our TPL5xxx or any other solution?

Regards,