Hello team,
My customer has questions for LMX2820 below. Could you please support to answer these?
- Could you share actual phase noise data around 11GHz? such as figure 3(6GHz) from datasheet.
- -236dBc/Hz as typ value of PN_PLL_Flat is specified in electrical characteristics table. Could you let me know measurement condition? or Does PN_PLL_Flat have dependency on f_PD?
- Calculating back PN_PLL_Flat from PhaseNoise of figure3 leads to -233dBc/Hz. So customer would like to understand the difference is due to measurement condition or f_PD dependency(electrical table is f_PD=100MHz while figure3 is f_PD=200MHz). If there is a way to improve the 3dB, customer would like to implement.
- Is there any way to perform continuous test for Lock testing with using EVM and TICS Pro?
Best regards,