Other Parts Discussed in Thread: LMK05318, LMK03318,
Team,
My customer has the following questions.
I plan to use six LMX2595 parts on one board. The overall size is important to me.
1. What is the best solution to provide 100 MHz reference clock to the parts?
2. I would like to connect SPI bus from six LMX2595 together but the chip doesn't have the registered address. What is the best solution to provide SPI bus to all LMX2595.
3. If I don't need manual ramping mode, can I leave RAMPCLK and RAMPDIR pins unconnected?
4. Can VccRF and Vcc be connected to the same 3.3V supply or do I need to connect them to two suppliers? On the datasheet, it says "single supply".
Regards,
Aaron