Other Parts Discussed in Thread: CDCE6214, TICSPRO-SW
(1) I want to use a single-ended crystal oscillator for Reference CLK. Is the following port connection correct?
・Connect the CMOS output single-end crystal oscillator (25MHz) to the "PRIREF_P" terminal (5pin).
・"PRIREF_N" terminal (6pin), "SECREF_P" terminal (1pin), "SECREF_N" terminal (2pin) are open
・Pull up the "REFSEL" terminal (4pin) to 3.3V
(2) I2C control cannot be used on my system. Is 100MHz (PCIe Ref-CLK) output just by applying power to CDCE6214?
(3) I want to use CDCE6214 in "Pin Mode". However, I don't know how to set it to "Pin Mode". What should i do?