Hi team,
The d/s mentions that SSC_SEL0/1 and FS-pin have internal pull-up.
1. When using at a high level, doesn't the customer need to connect an external resistor because there is the internal pull-up?
2. Is it okay to connect directly to GND when setting to Low level? ( Is there a problem with the internal pull-up resistor current? )
Regards,
Yamaguchi