Other Parts Discussed in Thread: PLLATINUMSIM-SW,
Hello,
For an application we need to have very fast switching and settling times.
May I ask you to please provide these numbers for the complete range (up to 20GHz). There is a mention of 20us VCO calibration speed, is there a connection to the switching time.
What is the mechanism to update the switching frequency with a deterministic latency?
Also, the datasheet doesn't speak much about the performance above 15GHz, could you please provide the phase noise spec.
2) In order to generate signals above 20GHz, can a frequency doubler be used?
3) What are the PFD spur levels? Also, near the carrier are there any other kind of spurious?
4) Is a frequency resolution of 1KHz possible?
5) How is output frequency accuracy calculated from the reference frequency stability/accuracy? Is an accuracy of 10KHz possible?
6) For the phase noise plots provided in the datasheet, I assume they are for a certain loop bandwidth? How is the switching/settling time calculated based on this?
Thank you for your help in understanding these points,