Other Parts Discussed in Thread: ADC12DJ3200,
Hi all,
I am using ADC12DJ3200 ADC interfaced via JESD204B with FPGA.
What is the sequence of registers to be written in order to generate continuous sysref?
I am generating 156.25 MHz from DCLK2 and 19.53625 MHz from SDClk3 and the same is generated from DClk12 and SDClk13. Both Dclk and SDClk are in LVDS standard with AC coupling capacitors.
The JESD link between ADc and FPGA fails randomly. Some times Sync pin is always low and sometimes Sync pin toggles.
Can you please help in identifying reason for that?
Also, Kindly give setting for below case,
I want Dclk to be generated when I configure LMK04828 and Sysref to be generated after I configure ADC and JESD Receive core.
Regards,
Naveen.A