Hello,
i'm using LMX2571 in frequency hopping mode with FSK I2S functions. It looks like switching noise is smaller when I reset the synthesizer (bit RESET in R0) and program all registers, than when I use the express setup (only the relevant registers are programmed and output power is on/off (OUTBUF_TX_PWR_F1, OUTBUF_TX_EN_F1). The datasheet says that the RESET function "Resets all the registers to the default values.", what internal functions (internal state machines) are involved in the RESET procedure? Can be still used express setup of synthesizer with achieving small noise levels?
Thanks,
Alex