Hello
I am using the LMK03806 with 100MHZ input from an OSC , VCO at 2400Mhz,
CLKOUT_0,1 open for one 100MHZ LVCMOS
CLKOUT_6,7 open for one 100MHZ LVCMOS
CLKOUT_10,11 open for 1200Mhz LVPECL (1.2V @ 240 ohm)
Please let me know if I calculated properly the LMK Power Dissipation:
Core: 122, Basic : 17.3, ClkOut Groups : 2 x 2.8, DIVIDORS (all 3 bellow 25) : 3x25.5, LVPECL : 30, LVCMOS : 2x 36.5
Total Current: 324mA
Total Power : 324 x 3.3 = 1070mW
Total LMK Power = Total Power - Ext_Res = 1070 - 40 = 1030mW (see Table 43 for 1.2V LVPECL @ 240ohm)
Thanks
Amnon