HI:
TI!
I have a problem with the lmk03806 input reference clock .
1.in the LMK03806 datasheet ,an external lvds reference clock is connected as follows ,
The 100R terminal resistance is in front of the ac coupling capacitance.
2.external reference clock source I select LMK61A2-100M00,(100MHZ,LVDS output)the output interface as follows:
the 100R terminal resistance behind ac coupling capacitor
3.My question
I would like to use lmk61a2-100m00 as the input reference clock for lmk03806,How to connect the terminal resistance ?