Other Parts Discussed in Thread: LMK04808, LMK04832, LMK04828
Hello,
I am currently making a high speed camera, and I would like the time delays between exposures (independently variable) to be controllable to within 1 nanosecond or better. If I am reading the datasheet correctly, the LMK03806 and similar clock generators can provide a very accurate clocks through the use of frequency dividers, and the SYNC contact can synchronize all the clocks.
Basically what I need is the clocks to all start running (or be reset) when I set the sync pin high to within a fraction of a nanosecond. The first rising edge of the fastest clock will trigger the first exposure, the rising edge of a slower clock will trigger next, etc. Does the synchronization have a high enough jitter that I will not be able to accomplish the proper timing?
If this clock will not work, would it be possible to recommend another device that will satisfy my requirement? Thanks for the help.