Hi,
My request to get lower frequency about 2.5 Mhz using the LMK04832.
At the BOM list of the LMK04832EVB the VCOs frequencies are: 1- 800Mhz up to 1030Mhz 2 - 1800Mhz up to 2200Mhz .
The schematics indicates that the basic VCO frequency in the PLL is 2942.19Mhz using reference VCXO =122.88Mhz .
Each of the 14 outputs can be divided by 1 up to 1023 . It means i can get minimum frequency of 2942.19\1024=2.87Mhz .
Are my calculations right?
What are the relations between the 2 VCOs listed in the BOM list to the 2942.19Mhz ??
Thanks in advance
Moshe Namer