Other Parts Discussed in Thread: LMX2571, LMX2572
Hello team,
Hope you are doing well and staying safe. When you get a chance please provide some feedback on below customer question:
In the LMX2582 datasheet, it states that input reference can be 5 to 1400 MHz. We used a 10MHz VCTCXO and noticed that this will not work.
There is only a doubler inline before the multiplier and the input for the multiplier is 40 MHz to 70 MHz. So, should the minimum value for input reference be 20 MHz as compared to 5 MHz?