Hi Team,
My name is Maki and work for Osaka office in Japan as a FAA.
I have an inquiry regarding CLKouts of LMH1983.
According to DS of LMH1983, the CLK generator has four PLLs for Simultaneous A/V Clock Generation.
and my customer is now planning:
Input: 27MHz, H/V/FID
Output 1: 148.35MHz or 148.5MHz (for Camera head transmission)
Output 2: 148.35MHz or 148.5MHz or 54MHz (refclk for 1 HDMI channel)
Output 3: 148.35MHz or 148.5MHz or 74.25MHz or 74.175MHz or 54MHz (refclk for 2 HDMI lines)
Is it possible?
and my customer wants to make sure that Output 1 is not interrupted when Output 2 or Output 3 are changed.
Best Regards,
Maki